SIMATIC HMI Basic Panels from Siemens are suited for various basic applications. They do not only allow comprehensive monitoring but also user-friendly controlling of installations and machinery. This saves both time and money. The SIMATIC HMI Basic Panels are available in different display sizes and with touch or key operation. The integrated software functions such as alarm logging, recipe management and trend functions are convincing.
SIMATIC HMI Basic Panels: Two generations with different advantages
There are two different generations of SIMATIC HMI Basic Panels. Each one has its own advantages.
SIMATIC HMI Basic Panels of the 1st generation convince not only with their easy handling but also with their proven quality and functionality. These panels are suited above all for less complex visualisation tasks, even where space is restricted. Where space is at a premium, the KP300 Basic mono PN device with its high-resolution display and key operation is a good solution. The projects created on these panels allow upward compatible transfer to the HMI Comfort Panels.
The SIMATIC HMI Basic Panels of the 2nd generation await with perfected HMI functions and an optimum process quality. The high-resolution dimmable colour display offering 65,000 colours and the new user interface guarantee even more user-friendliness. Configuration using the engineering software SIMATIC WinCC (TIA portal) helps to achieve excellent usability. Even if there is a change to other devices the projects created for a basic panel will not be lost since they can be easily transferred. Among the panels of the 2nd generation the panel KTP700 Basic PN is particularly suited for complex demands.
Automation24 offers Siemens SIMATIC HMI Basic Panels of the 1st generation and SIMATIC HMI Basic Panels of the 2nd generation. The panels of both generations can be used in PROFINET environments. A particularly good complement of SIMATIC HMI Basic Panels is the engineering software SIMATIC WinCC Basic in the TIA Portal.
At Automation24 you find SIMATIC HMI Basic Panels of the proven 1st generation and the innovative 2nd generation at very favourable prices. Select the panel suitable for your application today!