Before connecting a cable, the cables outer jacket is removed and the enclosed hook-up wires exposed. This process is called stripping. Thereafter, a small portion of insulation is removed from the end of the stranded conductors. The length of insulation to be stripped is, for example, determined by the dimensions of the insulated wire end ferrules, which are to be connected to the conductors.
Since it is of crucial importance in this process that the conductors are not damaged, the use of stripping tools is recommended.
Wire / Cable strippers from Weidmüller - practical helpers
An area of expertise for Weidmüller is the stripping of wires and cables.
For this purpose, the manufacturer has developed and produced professional wire / cable strippers which offer the following advantages in particular:
With the stripping tools from Weidmüller, different cable diameters can be processed conveniently and simply. They ensure a fault-free, precise and consistent stripping result without damage to the conductors. The stripping tools are durable and designed for daily use.
In Automation24's portfolio, you will find a selection of professional wire / cable strippers from Weidmüller in the work tools section for error-free cable processing. There are stripping tools for PVC, moisture proof or coaxial cables, stripping pliers as well as cable knives.
Weidmüller became well-known through its innovative stripping tool, Stripax®, and Stripax® ULtimate, with which halogen-free and UL as well as UL-like insulated conductors can be processed. Thanks to the self-adjusting blades and the 3-stage stripping function, particularly hard insulation is not a challenge for Stripax® ULtimate.
Ensure you are optimizing your operations and increasing the productivity of your company with Weidmüller work tools. All products are available in stock at the best prices - order today!